Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find information about how an ATV960 part number breaks down?
Issue:
ATV960 part numbers break down

Product Line:
Altivar 960 drives

Environment:
All

Cause:
Would like to know what each character in the part number designates

Resolution:
The ATV960 drives are customizable enclosed drives. Each character (digit or letter) or groups of characters in a drive's part number designates a particular characteristic (spec) of the drive. Details about each of these specs can be found in the attached ATV960 Installation Manual in Section 2 'Product Characteristics'.

For example: ATV960D18T4N2GAYAAN
ATV960 = Altivar 960 drive
D18 = horsepower size (25HP)
T4 = voltage class (460V)
N = normal duty
2 = UL marking
G = Type 1 General Purpose (NEMA 1)
A = Line Harmonic Mitigation (5% impedance)
Y = Includes Integral full-voltage bypass
A = Control Options (H-O-A, Speed Potentiometer)
A = Light options (Red Power On, Yellow Tripped, Green AFC Run, Yellow Auto)
N = Communication card (None)

Schneider Electric Saudi Arabia

Attachment(s)
ATV960 installation manual_ 2016.pdf [26.89 MB]