Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which Unity version supports the 140CPU65160S
Issue
Which Unity version supports the 140CPU65160S

Product Line
Quantum 140CPU65160S

Environment
Windows 10

Resolution
Support for the 140CPU65160S is only available with Unity 7.
Any version later than Unity 7 does not support the Quantum 140CPU65160S