How can we help you today?

In a Quantum PLC is %SW125 (which indicates the cause of a HALT) reset on a power cycle?

Issue
In a Quantum PLC is %SW125 (which indicates the cause of a HALT) reset on a power cycle?

Product Line
EcoStruxure Control Expert (former Unity Pro), Modicon Quantum

Environment
Unity Pro v12.0, 140CPU67160


Resolution
Attached is a chart with the results of various restarts on %SW125. a yes indicates the value is set to zero.

Schneider Electric Saudi Arabia

Attachment(s)
rtaImage.jpg [32.58 KB]
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
  • Product Documentation