Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change an Array of BYTEs to an Array of INTs or WORDs in the DIO scanner of a NOC in M340 configuration?
Issue

how to change an Array of BYTEs to an Array of INTs or WORDs in the  DIO scanner of a NOC in M340 configuration?.

Product Line
M340

Environment
Unity Pro, Control Expert



Resolution

The attached document explains the procedure.

Schneider Electric Saudi Arabia

Attachment(s)
Changing Data Types in DDDT M340 and BMXNOC.zip [118.8 KB]