Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the common mode filter for bearing current reductions for the ATV600 and ATV900 drives frame size six drives?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.



Resolution:
The part number is VW3A5506 and its value of inductance is 274.8 uH

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
Altivar Process ATV900_VW3A5506.pdf [93.6 KB]