Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Common mode filter for bearing current reductions for the ATV600 and ATV900 drives frame size three drives?
Issue:
Common mode filter for bearing current reductions for the ATV600 and ATV900 drives.

Product Line:
ATV600 and ATV900 drives frame size 3

Environment:
All

Cause:
Filter for bearing current reductions

Resolution:
The part number is VW3A5503 and its value of inductance is 120.0 uH

Schneider Electric Saudi Arabia

Attachment(s)
Altivar Process ATV900_VW3A5503.pdf [93.46 KB]