Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible in Unity pro to force %IW values directly from the Animation Table with M580?
Issue
Need to force analog input DDT in the M580.

Product line
M580, Unity pro , Control Expert

Resolution
It is possible now to force Analog inputs on M580 with unlocated data model (on Device DDT).
it will not be implemented on located data, because Schneider focus is on unlocated Data with M580.