Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is the gateway address not being displayed on M580 embedded web page?
Issue

Why  is the gateway address not being displayed on M580 embedded web page?

Configuring the gateway as shown below: 10.130.2.254




The embedded M580 webpage is displaying the gateway address: 0.0.0.0




Product Line

M580, Unity pro , Control Expert

Resolution

This is issue is reported on M580 firmware below or equal to 2.20. The issue is no longer present in firmware above 2.20