Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you read run status on the ATV630 and ATV930 drives using profinet telegram 1?
Issue:
Read run status on ATV630 and ATV930 drives using profinet telegram 1.

Product Line:
Altivar ATV630 and ATV930 drive

Environment:
All

Cause:
Status word for run is bit 2

Resolution:

The second word in the input table on the profinet side is for status.
bit 2 is the enable or run operation.

Bit 2

Profi