{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the drive read and display input line current on the ATV61 and ATV71 drives?
Issue:
Can the ATV61/ATV71 read and display supply current or input line current on the default display or in the Drive Menu under 1.2 Monitoring?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Displaying  input line current.

Resolution:
No you can not read the input line current on the display.  The drive will display motor or load current, however, it is not possible to display supply or line current.

Schneider Electric Saudi Arabia