Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to read variables directly from the M580 Safety CPU safe task using OFS.
Yes, OFS V3.61 allows to access in Read to the safe variables using prefix "SAFE" before (ex : SAFE.bool1). Write access is possible also, but only in "maintenance" mode.