Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does an Altivar Drive have to be enclosed in order to have a bypass?
Issue:
Wondering if an Altivar Drive have to be enclosed in order to have a bypass

Product Line:
All Altivar drives

Environment:
All

Cause:
Deciding whether an enclosure is needed

Resolution:
An Altivar Drive can be wired with a bypass whether it's mounted open-style or enclosed. If our drives are ordered with a bypass, they are sold in enclosures. However, a drive can be purchased, and the customer wire in a bypass circuit and mount it all in their own enclosure if they choose to do so. We offer many types of enclosed drives, with and without bypass, as well as our stand-alone drives.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: