Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In EcoStruxure Operator Terminal Expert (Vijeo XD v3.0), the Transfer Button is grayed and it is not possible to download a project to my Magelis HMI

Article available in these languages: Spanish

Issue
In EcoStruxure Operator Terminal Expert (Vijeo XD v3.0), the Transfer Button (located in the Buildtime Editor interface on the top menu bar) is grayed out and it is not possible to download a project to my physical Magelis HMI.

Product Line
EcoStruxure Operator Terminal Expert (Vijeo XD v3.0)

Resolution
If the Vijeo XD license is not activated, Transfer to a physical Magelis HMI will not be available (grayed out) in the Buildtime Editor interface on the top menu bar..
Run the License Manager and click on the "Task" menu. Select "Register license into my account ...". Then follow the instructions shown in the dialog box.
Once the registration procedure has been completed, delete the "Vijeo XD Trial" Activation ID.

Schneider Electric Saudi Arabia

Attachment(s)
Vijeo XD License Manager.PNG.png [27.15 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: