Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure the BMXNOM200 for 'Stop on Reception' using both CR and LF
Issue
How to configure the BMXNOM200 for 'Stop on Reception' using both CR and LF

Product Line
BMXNOM0200

Environment
Unity, Windows 10


Resolution
To configure the NOM serial port for the Stop on recption using both CR and LF, reference the example in the following screen capture.

ffff