Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a good source of information for finding part numbers for shorting contactors for the ATS48?
Issue:
Information on part numbers for ATS48 shorting contactors.

Product Line:
ATS48

Environment:
All

Cause:
Customer needs a shorting contactor for installation with an ATS48

Resolution:
The ATS48 Installation Manual (attached) is a good reference. There is a table on page 84 of the manual which lists part numbers for shorting contactors, isolation contactors, fuses, etc, listed by ATS48 part number.

ATS48 Shorting Contactors list

Schneider Electric Saudi Arabia

Attachment(s)
ATS48 installation guide.pdf [1.3 MB]