Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to use temperature input on encoder card in ATV930?
Temperature input configuration of VW3A3423 card is available in menu Complete setting - generic monitoring - thermal monitoring. You can configure thermal sensor type, threshold and reaction.