Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use old BSH140.M motor with LXM32? Is the a performance table?
Yes, there is Lexium torque-speed tool in attachment where you can select BSH1401M/BSH1401M2/BSH1401M3/BSH1401M4 + LMX32

Schneider Electric Saudi Arabia

Attachment(s)
lexium servo - torque speed curves - v2.04.xls [752.5 KB]