Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What IP address does M580 DHCP server use?
Issue

Customers are often confused whether which M580 IP address (main IP or IP A) is used as DHCP server IP address.

Product Line

M580


Resolution

The DHCP server uses the main IP of the CPU to serve the CRA as well as the X80 HART modules.