Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the OLN parameter mean on the ATV21 and ATV212 drives?
Issue:
OLN meaning on the ATV21 and ATV212 drives.

Product Line:
Altivar ATV212

Environment:
all

Cause:
Motor overload function

Resolution:
OLN is the motor overload characteristics for self cooled, force cooled etc.   The factory default is 0 for self cooled motor.