{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The Self-test status is unavailable on the LCD display of an SRT UPS

Article available in these languages: Russian

Issue: The Self-test status is unavailable on the UPS display.

selftest

Product line: SRT 5 to 10kVA models

Cause: When initiating a Self-test using the UPS front panel, the Self-test status is not updated on the display, regardless of Self-test results.

Resolution: This is a cosmetic issue only, and does not affect the UPS functionality. The Self-test can still be performed and the results are available in the NMC Event logs. To resolve this, perform a UPS firmware upgrade to the latest firmware revision available in FA279197 .

Schneider Electric Saudi Arabia