Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you retrieve data from the A9MEM3155 modbus meter wireless using a Modbus to WiFi converter?
We recommend using a standard tested SE solution like COM'X with a Wifi dongle, which can be connected to iEM3155 over Modbus RTU and COM'X will send the data of the meter over Wifi.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: