Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why can I not see Display Configuration Menu on ATV61 drives?
Issue:
Display Config under the Main Menu is not visible.

Product line:
Altivar 61, ATV61

Environment:
n/a

Cause:
n/a

Resolution:
To see the Display Config menu, the drive must be in Access Level of Advanced or Expert. You also have to have the Password function deactivated or turned off.