Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the ATV320 24Vdc power supply rating?

Article available in these languages: Spanish

Issue:
Planning external uses for the available 24Vdc power supply from the ATV320.

Product line:
ATV320, Altivar 320

Environment:
n/a

Cause:
n/a

Resolution:
The Altivar 320 power supply is rated for 100mA load.  Tolerance of the voltage supply is -15% to +20%.
Note that the logic inputs use 7mA each.