Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
The Vigi module for Compact NSX is type A or AC?
The Vigi module for Compact NSX devices is Type A according to IEC 60755, immunity to DC components up to 6mA.