Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you use a DV/DT motor protecting filter on a ATV320 drive running a permanent magnet synchronous motor?
Issue:
ATV320 using a DV/DT filter to run a permanent magnet synchronous motor

Product Line:
ATV320

Environment:
All

Cause:
DV/DT filter on synchronous permanent magnet motor.

Resolution:
Yes, you can use a DV/DT motor filter using a PM synchronous motor.