How can we help you today?

Can the Panelboard-style covers for Riser Panels be used when panel is converted to a main breaker panel?

Issue:
Panelboard-style covers be used when the panel is converted to a main breaker panel

Product Line:
Load Center

Environment:
QO Riser Panel

Resolution:
Panelboard-style Covers for Riser Panels cannot be used when panel has been converted to a main circuit breaker panel.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre