Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What energy parameters are measured by PM1130H meter ?

Issue:
Customer would like to understand the energy parameters that are measured by the PM1130H meter

Product Line:
PM1130H meters

Environment:
Hardware

Cause:
Customer cannot obtain documentation for meter

Resolution:
The meter provides uni-directional, 2-quadrant, Class 1 / Class 0.5 accurate energy metering. The meter stores accumulated value of any one of the selected energy from active, reactive, or apparent energy in nonvolatile memory:


• Delivered (Utility): kWh, kVARh, kVAh
• Delivered (Alternate Source): kWh, kVARh, kVAh
• Total (Utility + Alternate Source): kWh, kVARh, kVAh
Under the condition when Source 1 = Utility and Source 2 = Genset or DG.