Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the default serial port settings in PM1130H meter ?

Issue:

Customer wants to know the default serial settings on the PM1130H meter

Product Line:

PM1130H meter

Environment:

Hardware/Devices

Cause:

Customer would like to know configurations and cannot access for any reason


Resolution:

The meter is factory-configured with the following default serial communications settings:

Protocol = Modbus RTU
• Address = 1
• Baud rate = 19200
• Parity = Even

Documentation: EasyLogic PM1130H Dual Source meters