Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is imbalance factor calculated in EOCR-i3DM (Z, S, 420) / iFDM (Z, S, 420) for current imbalance protection
Imbalance factor for EOCR-i3DM (Z, S, 420) / iFDM (Z, S, 420) is calculated as follows:

Imbalance factor (%) = (Imax phase - Imin_phase) / Imax_phase x 100%