Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to configure one port on the HMIGTU to communicate with a PLC on one subnet, and the other port to communicate to a PLC on a different subnet?
Issue:
Can the HMIGTU communicate to devices on two different subnets?

Product Line:
HMIGTU

Resolution:
It is possible for an Magelis HMIGTU (HMIG3U or HMIG5U) to communicate to two PLC's on a different subnets.

I have attached a screen capture on how you would configure Vijeo Designer.  The Runtime will automatically route the device to the Ethernet port on the correct subnet.

Schneider Electric Saudi Arabia

Attachment(s)
HMIGTU_Different Subnet comm.jpg [106.36 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: