Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where do you wire in the DB resistor on the ATV320 drive?
Issue:
Wiring DB resistor on an ATV320.

Product Line:
ATV320 with C and B suffix

Environment:
All

Cause:
Wiring terminations for adding a DB resistor on the ATV320 drive.

Resolution:
The ATV320.....B   DB resistor terminals are PBe and PB.

The ATV320.....C   DB resistor terminals are PO and PB.

See the attached documents on terminations and min resistance.


Schneider Electric Saudi Arabia

Attachment(s)
PBe to PB for the B suffix versino ATV312.JPG.jpg [115.58 KB]
PO to PB for the C suffix versino ATV312.JPG.jpg [115.17 KB]
Min resistance values for the ATV320 drives.JPG.jpg [158.68 KB]