Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does ATV600 have fire mode?

YEs, with firmware 1.8 or newer there is forced mode function, configurable using parameters INH, INSH, INHR. Printscreen enclosed.
Description of the function is mentioned in newest manual (ATV600_Programming_Manual_EN_EAV64318_xx)

Schneider Electric Saudi Arabia

Attachment(s)
Forced mode.jpg [156.36 KB]