Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we copy the program from ATV61 to an ATV71 using the ATV61's keypad?
Issue:
Copying the program from ATV61 to an ATV71 (or from an ATV71 to an ATV61) using the VW3A1101 keypad

Product Line:
Altivar Drives

Environment:
All

Cause:
Replacing an ATV61 with an ATV71 and wanting to copy the program

Resolution:
No.
You cannot directly transfer a program from one series drive (ATV61) to a different series (ATV71).
The parameters and basic settings may be the same, but there are differences in the memory map that will not allow this.
The easiest way to do this is use SoMove to display the ATV61 program. Open a second instance of SoMove and create a new project for the ATV71.
Then manually enter the settings in the ATV71 program.
Copying from drive to drive using the keypad or SoMove can only be done within the same product family.