Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is the Local/Remote selection not showing up under the R1 selection table in the IO relay configuration?
Issue:
The Local/Remote configuration on IO Relay.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
They want the R1 relay to show Local or Remote status

Resolution:
Check your firmware version it needs to be version V1.6IEXX or above for this feature to be available.