Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Whether third party servomotors can be used with LXM32 servo drives
Third party motors are only possible via an additional analog encoder module or resolver module on slot 2 on Lxm32M and the motor encoder should only be resolver or sincos.