Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video : Configuration of BMXNOM0200 in a EIO to communicate with a serial slave
Issue
Configuration of BMXNOM0200 in a EIO to communicate with a serial slave

Product Line
EcoStruxure Control Expert (formerly known as Unity Pro), Modicon M580

Environment
Windows 10 version 1902, Unity Pro v13.1, BMEP585040, BMXNOM0200

Resolution
The BMXNOM0200 can be used on a remote drop (EIO) to read/write data from a modbus serial slave and this video shows the configuration of the ADDMX and READ_VAR function blocks to read a value from a modbus serial slave.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre