Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the recommendations for connecting PTC to the Altistart ATS48?
Issue:
What are the recommendations for connecting PTC to the Altistart ATS48?

Product Line:
ATS48

Environment:
All

Cause:
Wiring

Resolution:
Manual shows the following;
PTC1, PTC2 -  Total resistance of probe circuit: 750 Ω at 25 °C/77 °F
• For example, three 250 Ω probes in series
1
PTC monitoring also needs to be enabled in the programming:
1

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)