Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we offer a NEMA 3R flange kit on the ATV600 and ATV900 process drives?
Issue:
Are the NSYPTDS5 Flange kits NEMA 3R rated?

Product Line:
NSYPTDS5

Environment:
All

Cause:

Resolution:
Flange kit  NSYPTDS5 + ATV630/ATV930 drive association has not been approved to be NEMA but has qualified to be IP55 only conforming too IEC standards.