In a Quantum PLC what happens to the value of %SW125 (which indicates the cause of a HALT) on a power cycle?
Issue
In a Quantum PLC what happens to the value of %SW125 (which indicates the cause of a HALT) on a power cycle?
Product Line
EcoStruxure Control Expert (former Unity Pro), Modicon Quantum
Environment
Unity Pro v13.1, 140CPU67160
Resolution
Attached is a chart with the results of various restarts on %SW125. a yes indicates the value is set to zero.
Released for: Schneider Electric Saudi Arabia