Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What meters can measure a 400 Hz system?
Product Line
ION9000
PM8000
ION7400
CM4000

Environment
400 Hz System

Resolution
The ION9000, PM8000, ION7400, and CM4000 are all capable of measuring a 400 Hz system.

The supported measurements are Voltage, Current, Frequency, Power, and Energy while Total Harmonic Distortion, Harmonics, etc are not supported. Demand values and alarming are also expected to work correctly.

For more information on the PM8000 capabilities, see FA303197.