Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PowerChute Business Edition v9.5 and above displays Linux RPM package public key error
Issue:
This Knowledge Base article outlines the steps required to resolve the warning message showed when installing PowerChute Business Edition v9.5 + using rpm on Linux.

Product:
PowerChute Business Edition version 9.5 and above

Environment:
Linux

Cause:
PowerChute Business Edition’s RPM package for Linux is signed by the GNU Privacy Guard (GPG). If GPG’s public key is not installed, the above warning message will be shown when installing the PowerChute Agent. In order to prevent this warning from appearing, please install the public key on your system.

Resolution:
See attached PDF

Schneider Electric Saudi Arabia

Attachment(s)
PowerChute Business Edition v9.5 and later displays Linux RPM package public key error.pdf [151.77 KB]