Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which target are compatible for the Site Manager of Ecostruxure Secure Connect Adviser?
SiteManager (iPC/HMI)
The SiteManager software has to be running on the display unit for providing remote access to that display unit and subnetwork(s), if any, of that display unit.
Depending on the type of display unit, the SiteManager software is either:
  • SiteManager Win OS: pre-installed as a service (or to be installed as a program) on Windows OS of HMIs that are running Windows OS
  • SiteManager Embedded: embedded within the project RunTime of HMIs that are running another OS than Windows OS
  • SiteManager Linux

SiteManager Linux OS
The only one supported model compatible for Linux is HMIBSCxx

SiteManager Win OS
For a list of hardware models of display unit running a Windows OS that support EcoStruxure Secure Connect Advisor offer, please refer to the list of supported models bellow.


The new iPC model as HMIBMO and HMIBMI are also supported

SiteManager Embedded
For a list of hardware models of display unit running another OS than a Windows OS that support EcoStruxure Secure Connect Advisor offer, please refer to the list of supported models bellow.

Note: Vijeo XD does not support "HMIGTO terminal" models.