How can we help you today?

EF SHR unexpected behavior

You are using Unity Pro V11 or higher and option Optimized code is selected (Project Settings / Build settings / Optimized code)
You are using M580 High End CPU, BMEP585040, BMEP586040 or BMEH586040.
In such configuration because these CPU used a new compilator managing differently data signed and data unsigned the result of the EF operation is unexpected.

A workaround exists, use the EF SHR_INT or use only UINT data type when using a SHR. A comment will be added on the Unity Pro Read_Me.

NOTA This behavior doesn’t exist with other M580 PLCs references.

Schneider Electric Saudi Arabia
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
  • Product Documentation