Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the ATV320 24Vdc logic input loading?
Issue:
What is the consumption on the ATV320 digital inputs?

Product Line:
ATV320

Environment:
All model numbers, all serial numbers

Cause:
Calculating external power supply requirements

Resolution:
The ATV320 digital inputs, DI1 thru DI6, consume 7mA each.  The STO input consumes 16mA.