Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the functions of passive filters for variable speed drives ATV600?
Passive filters are used to obtain total harmonic distortion of less than 10% or 5%.
Reactive power increases at no load or low load.
To help reduce this reactive power, the filter capacitors can be disconnected (see the diagrams on our website  www.schneider-electric.com).
Passive filters provide IP 20 protection.