Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we assign the auxiliary functions like buchholz trip,SF6 low, Pressure trip, pressure alarm in SEPAM T87 relay?
Description:
Auxiliary functions like buchholz trip,SF6 low, Pressure trip, pressure alarm assignment possibility in SEPAM T87 relay

Product family:
SEPAM T87 relay

Resolution:
Yes ,All the above functions can achieve through SEPAM 80 series relay .All these inputs are available as standard assignment in our SEPAM SFT 2841 software (under Logic I/Os)