Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video : How to Diagnose a BMENOS0300 by Device DDT?
Issue
The BMENOS0300 includes 16-Byte DDDT, which you can interrogate to diagnose the status of the module.

Product Line
Modicon M580, BMENOS0300, EcoStruxure Control Expert (formerly Unity Pro)

Environment
Unity Pro v12, BMENOS0300, BMEP581020 v2.50

Resolution
This video will show how to read/interpret the 16-Byte DDDT from BMENOS0300 to diagnose the status of the module.