Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you confirm whether SEPAM 80 will support for IEC 61850 Edition 1 & Edition 2

Description:
Whether SEPAM 80 will support for IEC 61850 Edition 1 & Edition  2?

Product family:
SEPAM 80

Resolution:
Yes , SEPAM 80 will support for IEC 61850 Edition 1 & Edition  2.

However, thanks to verify with the selected model as per the order code with your local pre sales/PAE/FO team.