Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the HMIS5T and the HMISTU655 or HMISTU855?

Article available in these languages: Spanish

Issue:
The part numbers of the HMISTU series are not self explanatory. What are the differences between the models?

Product Line:
HMISTU series
HMISTU655, HMISTU855, HMIS5T, HMIS65, HMIS85

Resolution:
Here is a description of what the HMISTU part numbers consist of.
If you order these part numbers:

[After March 2012]
Ordered Part Number: HMISTU655:

In the box there are two components:
1) HMIS5T back module (the sticker says HMIS5T)
2) HMIS65 (3.5" TFT color screen - sticker label reads HMIS65)

Ordered Part Number HMISTU855:
In the box, there are two components:
1) HMIS5T back module (the sticker says HMIS5T)
2) HMIS85 (5.7" TFT color screen - sticker label reads HMIS85)

Ordered Part Number HMIS5T:
Only the HMIS5T back module will be in the box

Ordered Part Number HMIS65:
Only the HMIS65 3.5" TFT color screen will be in the box

Ordered Part Number HMIS85:
Only the HMIS85 5.7" TFT color screen will be in the box

The HMIS5T back module can use EITHER the HMIS65 or HMIS85 interchangeably.

[Prior to March 2012]
Ordered Part Number: HMISTU655:
In the box there are two components:
1) HMISTU655 back module (the sticker says HMISTU655)
2) HMIS65 (3.5" TFT color screen - sticker label reads HMIS65)

Ordered Part Number HMISTU855:
In the box, there are two components:
1) HMI855 back module (the sticker says HMISTU855)
2) HMIS85 (5.7" TFT color screen - sticker label reads HMIS85)

Ordered Part Number HMIS65:
Only the HMIS65 3.5" TFT color screen will be in the box

Ordered Part Number HMIS85:
Only the HMIS85 5.7" TFT color screen will be in the box

The Back Modules (with sticker labeled "HMISTU655" and "HMISTU855") are NOT INTERCHANGEABLE with the HMIS65 and HMIS85 screens.


[How to read the Serial Number to check manufacture date]
On the back of the HMI, there will be a sticker with a "SN" number.

For example: WXS1Bxxxx1223xxxx
Digits 10 and 11 (from the left) indicate year of manufacture (12 = 2012)
Digits 12 and 13 (from the left) indicate week of the year (23 = 23rd week of the year - which is June 4th)


[Software Compatibility Rules]
The HMIS5T back module has 64MB of DRAM and 32MB of application flash.  This is twice the amount of memory from the first generation of HMISTU.

HMIS5T back module requires Vijeo Designer V6.0 SP3 to select the HMIS5T in the configuration. Note that all HMIS5T's manufactured after November 2018 will require Vijeo Designer V6.2 SP7. There will be a label on the rear module indicating this.

In Vijeo Designer, always select the correct target type as listed on the label of the rear module. Do not use the target type model HMISTU655 or HMISTU855 unless your label indicates that.

The suffix letter 's' in HMISTU655s and HMISTU855s indicates that the Vijeo Designer Limited disk is included with the package.  No software registration is needed for the HMISTU.