Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PM5500 Series Firmware Version 2.5.2 and Release Notes

Issue
Looking for new firmware version

Product Line
PM5500 series meter

Environment
Firmware upgrade

Cause
Need to upgrade PM5500 series meter to version 2.5.2

Resolution
Release notes: PM5500 firmware upgrade to address new and updated features.

Updates: This version implements EtherNet/IP, the name given to the Common Industrial Protocol (CIP), as implemented over standard Ethernet (IEEE 802.3 and the TCP/IP protocol suite). EtherNet/IP is enabled by default in firmware v2.5.2.

Note: This firmware update is intended for PowerLogic PM5560 and PM5563 meters

Please see the following link for more information regarding the PM5560 / PM5563 V2.5.2 Release